This reference design has been
developed to target applications that require lower power consumption, lower BOM
cost, as well as, smaller sensor size. Following are the main design
considerations:
- Low power consumption
The design consumes less power for applications
like motion and presence detection, gesture recognition, and so on. - Low cost
The design has a reduced BOM (bill of material)
cost. - Small overall size
The reference design has a small form factor to
allow the same to be placed into space constrained environments such as TVs,
monitor, and digital picture frames. In these and similar end equipments, the
radar needs to be placed in the bezel region. Therefore, the antenna region must
be optimized to fit into an area which nowadays can often be less then 2 cm in
width. - Antenna FoV and angle
resolution
The antenna design has a wide
FoV and a good angular resolution that helps covering larger areas.
With these design considerations, the
reference design has been developed with the following communication interfaces:
UART, SPI, and I2C. This section describes how different components used in this
design supports the requirements.