TIDUFB0 July 2025
To evaluate DALI 103 (303) communication, the following hardware components are required:
Figure 3-1 depicts a comprehensive system diagram, illustrating the connections between two LaunchPads. The LaunchPad on the left serves as the Device Under Test (DUT), featuring a PIR sensor and external 24VDC supply enabled using the J1, J6, and J7 jumpers. On the right side, a separate LaunchPad is employed to transmit commands to the DUT during run time, facilitating a precise testing procedure.
This setup is designed to validate that the DUT accurately receives and responds to commands from the DALI bus.