TIDUFC1A November   2025  – February 2026

 

  1.   1
  2.   Description
  3.   Resources
  4.   Features
  5.   Applications
  6.   6
  7. 1System Description
    1. 1.1 Key System Specifications
  8. 2System Overview
    1. 2.1 Block Diagram
    2. 2.2 Design Considerations
    3. 2.3 Highlighted Products
      1. 2.3.1 ADS127L21B
      2. 2.3.2 REF81
      3. 2.3.3 REF54
      4. 2.3.4 RES21A
      5. 2.3.5 THP210
      6. 2.3.6 OPA828
  9. 3System Design Theory
    1. 3.1 Range Selection
    2. 3.2 Linearity and Low-Noise Signal Chain
    3. 3.3 Calibration
    4. 3.4 Additional System Design Considerations
  10. 4Hardware, Software, Testing Requirements, and Test Results
    1. 4.1 Hardware Description
      1. 4.1.1 PCB Interface
      2. 4.1.2 Input Multiplexer
      3. 4.1.3 Gain Multiplexer
      4. 4.1.4 Power Supplies
      5. 4.1.5 Clock Tree
    2. 4.2 Software Requirements
    3. 4.3 Test Setup
    4. 4.4 Test Results
      1. 4.4.1 Integral Nonlinearity Measurements
      2. 4.4.2 Noise Simulation
      3. 4.4.3 Noise Measurements
      4. 4.4.4 Conclusion
  11. 5Design and Documentation Support
    1. 5.1 Design Files
      1. 5.1.1 Schematics
      2. 5.1.2 BOM
    2. 5.2 Tools
    3. 5.3 Documentation Support
    4. 5.4 Support Resources
    5. 5.5 Trademarks
  12. 6About the Author
  13. 7Revision History

Test Setup

The PCB is evaluated through the PHI board connected to a computer running the ADS127L21EVM-PDK-GUI software.

The following components are required for noise and linearity tests:

  • Reference design PCB
  • PHI controller card
  • PC running ADS127L21B software
  • ±15V power supplies
  • Low-noise dc source
  • 8.5-digit DMM

Follow the steps shown in Figure 4-8 to measure dc voltages.

  1. Connect the PHI controller to the PCB
  2. Connect ±15V power supplies to the PCB using J21
  3. Connect an 8.5-digit DMM between the input at J2 and GND_SENSE (TP19)
  4. Use J4, J5, and J6 to select the input signal
  5. Use J12 and J13 to select the gain of the programmable gain amplifier
  6. Connect a precision DC source to the SMA input connector, J1
TIDA-010970 Test Setup for Measuring dc Voltages With TIDA-010970Figure 4-8 Test Setup for Measuring dc Voltages With TIDA-010970

Use the SMA connector to connect the precision dc source to the signal chain input with the shortest connections possible. SMA connectors reduce the noise coupled into the signal chain compared to pin headers, allowing for higher-accuracy measurements. Use an 8.5-digit DMM because the reference design is intended to measure with 7.5-digit accuracy. Using a meter with higher resolution than the target resolution of the signal chain is important. Assessing whether the signal chain has met the target resolution is not possible if the meter has the same resolution because the meter has error.

Calibrating and taking measurements with respect to a GND_SENSE test point (TP19, TP20, TP42, TP43, or TP44) is important. REF81 is referenced to the GND plane. Small resistances on the GND plane can cause measurable voltage drops because REF81 draws significant current, which impacts measurement accuracy.

All the measured test results are taken with respect to a GND_SENSE test point.