The following steps describe how to
collect sensor data using the BoosterPack together with Edge AI Studio. These
instructions are demonstrated using the MSPM0G5187 EVM as the reference platform.
However, other TI EVMs can also support sensors from the BoosterPack, and
compatibility is continuously being expanded.
Detailed documentation for data
collection with MSP devices is available from the tida_010997_data_capture ReadMe file.
- Hardware Setup:
- Connect the BoosterPack
to the LP-MSPM0G5187 LaunchPad™
Development Kit
- Make sure jumper J7 on
the BoosterPack is set to 1:2
- Build and flash the
tida_010997_data_capture example from the MSPM0
SDK to the MSPM0G5187
- Data Collection:
- Launch the CCStudio™ Edge AI Studio on your host PC
- Create a Time-series
Classification project and navigate to the Capture tab
- Make sure the correct COM
port is selected and baud rate is configured to 115200bps
- Verify the status bar
displays Hardware connected
- Select the appropriate
sensor, set the sample count and sample label, and select Start
Capture
- Data is saved in CSV
format