Eine Version auswählen
PROCESSOR-SDK-LINUX-RT-K2G
Linux-RT Processor SDK for K2G
K2G EVM Linux SDK (64-bit Binary)
Code Composer Studio IDE for Windows Host
Code Composer Studio IDE for Linux Host
Only used when creating an SD Card on Windows
Standalone ARM Toolchain - ARM GCC 8.3 2019.03 hard-float toolchain
K2G Linux SDK BSP Source Code
K2G Linux SDK prebuilt BSP binaries and root filesystem
K2G Linux SDK Arago source downloads
Quick Start Guide that was included in the EVM kit
Quick Start Guide that was included in the EVM kit
Produkte
Audio- & Radar-DSP-SoCs
Dokumentation
Instructions for creating an SD Card with Linux
Instructions for creating an SD Card with Windows
Link to Release Notes for Processor SDK Linux
Getting Started Guide
Link to the online Software Developers Guide which has the latest content
Software Manifest of Components Inside the SDK
Versionsinformationen
More Information If you'd like more information on all of these choices, please refer to the Processor SDK Linux Getting Started Guide (GSG) below or the latest version here . For a complete overview of the SDK, please refer to the Processor SDK Linux Software Developer's Guide (SDG) below or the latest version here .