SBASAQ5A june 2023 – august 2023 AMC3311
PRODUCTION DATA
Do not leave the analog input (IN pin) of the AMC3311 unconnected (floating) when the device is powered up on the high-side. If the device input is left floating, the bias current can generate a negative input voltage that exceeds the specified input voltage range, causing the output of the device to be invalid.
Do not connect protection diodes to the input (IN pin) of the AMC3311. Diode leakage current can introduce significant measurement error especially at high temperatures. The input pin is protected against high voltages by the ESD protection circuit and the high impedance of the external restive divider.