SLVSCJ5B December 2015 – June 2020 TPS7H3301-SP
PRODUCTION DATA.
Depending on the trace impedance between the VLDOIN/VDDQ bulk power supply to the device, a transient increase of source current is supplied mostly by the charge from the VLDOIN/VDDQ input capacitor. Use a 150-μF (or greater) tantalum capacitor in parallel with a 4.7-µf ceramic capacitor to supply this transient charge. Provide more input capacitance as more output capacitance is used at VTT/VO.