JAJSPF5 April 2024 ADS9813
ADVANCE INFORMATION
Select the desired register bank by writing to register address 0x03 in register bank 0. Register read access is enabled by setting SPI_RD_EN = 1b and SPI_MODE = 1b in register bank 0. As illustrated in Figure 6-10, read registers by using two 24-bit SPI frames after the SPI_RD_EN and SPI_MODE bits are set. The first SPI frame selects the register bank. The ADC returns the 16-bit register value in the second SPI frame corresponding to the 8-bit register address.
As illustrated in Figure 6-10, the steps to read a register are: