JAJSSC7 December 2023 TPSI3100
ADVANCE INFORMATION
The total error for the alarm or warning indicator is similar to the over-current protection total error except the error contribution due to the resistor divider does not affect the total error.
The error contribution due to the current sense amplifier offset is increased since the load current being detected is reduced.
As before, it is assumed that all error contributors are independent variables, so that the total expected error adds in a root mean squared fashion as follows: