JAJSMK4A February 2017 – May 2021 CC3120
PRODUCTION DATA
When a device restart is required, the user may either issue a negative pulse on the nHIB pin (pin 2) or on the nRESET pin (pin 32), keeping the other pulled high, depending on the configuration of the platform. In case the nRESET pin is used, the user must follow one of the two alternatives to ensure the reset is properly applied:
To ensure a proper reset sequence, the user has to call the sl_stop function prior to toggling the reset.