JAJU528B August 2022 – January 2023 OPA388-Q1
Figure 3-36 remains true if there are no capacitors between high-voltage lines to chassis ground.
By using Figure 3-36, the designer can identify the type of isolation error in the HEV or EV system. First, identify the isolation error. To classify the severity of the error, perform an analysis to implement the prevention mechanisms. Calculating the isolation leakage current can be complex if using capacitors from high-voltage lines to the chassis ground, which is a step to improve the electromagnetic compatibility (EMC) of the system. Maintain the look-up table or equations for the expected isolation voltages and leakage currents, which change to temperature. Highly precise analog components must be used for measurement circuits to identify and analyze isolation errors.