JAJU528B August 2022 – January 2023 OPA388-Q1
High-voltage measurement is required to calculate the isolation leakage current. In TIDA-01537 , the AMC1301-Q1 device is used to perform these measurements. The AMC1311B has a high input resistance, a 2-V input range, and can also be used for high-voltage measurements.
As Figure 2-11 shows, the Rsh monitoring resistor is placed in series to a high-ohmic potential divider network. Voltage measurements are performed with a floating ground of the AMC1301-Q1. The OPA320-Q1 device is used to amplify the signal range and give a single-ended output to an MCU or logic interface. The AMC1301-Q1 can measure a bidirectional signal of ±250 mV. In HEV or EV motors, battery voltages are only in the positive range, so the usable range of the AMC1301-Q1 is 250 mV. A potential divider network must be chosen in such a way that the voltage drop in shunt resistance must be ≤ 250 mV at the maximum battery voltages.
Use Equation 5 to calculate the high battery voltage.
where
Equation 5 is a simple equation that does not consider the influences of bias currents or offset voltages, which can lead to deviations in measurements.