SLVAFL4 august   2023 TPS61299

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Introduction of Smart Watch Fast Transient Performance Requirements
  5. 2TPS61299 Fast Transient Performance Introduction
    1. 2.1 Fast Transient Mode Setting
  6. 3Standby Time Calculation
  7. 4Test Report Based on TPS61299 Solution
    1. 4.1 Load Transient Test for TPS61299 and TPS61099
    2. 4.2 Efficiency and Load Regulation
    3. 4.3 Output Ripple Test for TPS61299 and TPS61099
  8. 5Conclusion
  9. 6References

Introduction of Smart Watch Fast Transient Performance Requirements

In the smart watch application, the LED shines at a repetitive rate on the wrist, which reflected from the blood in the artery and veins gets modulated according to the oxygen content in the blood. According to the sampling theory, LED needs to flash at the frequency of 50 Hz at least to sample the signal range from 0.5 to 10 Hz relatively accurately. Since the current in LED ramps from 0 to 200 mA during hundreds of nanoseconds, the undershoot of the Output voltage is extremely large, as is shown in Figure 1-1.

If the sampling begin before output voltage return to normal value, the data accuracy is degraded extraordinarily. For example, the PSRR and SNR decreases dramatically. Hence the sampling is expected to trigger until the output voltage settles to target value, which waiting period is denoted as ttran and the sampling time is tsample( which is definitely customizable). This settled value is the same across all the sampling periods and the LED can be turned off after the tsample. Thus the minimum tPWM time can be calculated by ttran plus tsample. All through the tPWM period, the LED current source needs to be always on, which dominates the power consumption.

GUID-20230703-SS0I-TCGT-ZBWW-HQTNSQ6QVPW1-low.svgFigure 1-1 Typical Transient Response
GUID-20230703-SS0I-VPTB-6ZWS-D0S3ZZF58C4R-low.svgFigure 1-2 Fast Transient Response

Assuming the sample times being equal, with fast transient performance shown in Figure Figure 1-2, the ttran can be reduced from 100 us to 10 us, thus the period of Led_PWM can be reduced as well, denoted as tPWM. With reducing LED light time, the system reduces energy consumption and improves its efficiency.