SNOAA35D April 2023 – December 2023 LM2901 , LM2901B , LM2901B-Q1 , LM2903 , LM2903-Q1 , LM2903B , LM2903B-Q1 , LM339 , LM339-N , LM393 , LM393-N , LM393B , LM397 , TL331 , TL331-Q1 , TL331B
In early 2022, TI made changes to the device top markings company-wide, and not just specific to the LM339 family. This change was covered in PCN# 20211123004 for most of the LM339 family.
The left photo is the previous bar style marking, and the right photo is the new dot style marking.
The package marking changes are:
These label changes are gradually being applied across TI, and is possible to get a mix of the two device marking styles in large orders. The marking changes do not directly indicate which die is used, and it is still possible to get a classic die with the new top marking style.