SNOAA35D April 2023 – December 2023 LM2901 , LM2901B , LM2901B-Q1 , LM2903 , LM2903-Q1 , LM2903B , LM2903B-Q1 , LM339 , LM339-N , LM393 , LM393-N , LM393B , LM397 , TL331 , TL331-Q1 , TL331B
A commonly misinterpreted specification is the Maximum Input Current or Input Current specification as listed in the Absolute Maximum Table. For this family, the specification can be as high as 50 mA (typically listed as -50 mA).
This current is actually the maximum current that can be passed through the reverse biased substrate diode without damage, though the specification does not imply proper operation at that time. This current is seen when a negative voltage is applied to the input attempting to pull the input below the GND pin (-0.5 V to -1 V). This specification sets a limit on the current as mentioned in the previous section on Negative Input Voltages. At 50 mA, improper operation and malfunctions are possible. TI still recommends keeping the current to below 10mA or less.
This specification does NOT relate to a maximum input bias current. When the input voltage is within proper specified operating range (0 V to Vcc-2 V), the input current can be within the Electrical Specification Tables for maximum bias current (<500nA) and must never approach the milliamp range under normal operation.