SNVU851A November 2023 – January 2024
Texas Instruments provides a simple to use LP87725-Q1 GUI tool to enable, configure, and evaluate the various features of the LP87725-Q1 device on the EVM. Please refer to the GUI README.md file in the GUI tool's Help->View README.md tab for a more detailed description of this tool.
The GUI runs on most PC platforms and requires a USB port for connecting the EVM to the host computer. The EVM USB connector is type-C and a type-A to type-C cable is provided along with the EVM to connect to the host computer. EVM gets automatically connected to the GUI after the USB cable is connected and manual assignment of COM port is not necessary. If Hardware not Connected displays on the bottom left of the GUI, clicking Click to connect to hardware icon next re-establish the connection. The GUI uses the ACCtrl COM port which can be found from the device manager of the operating system.