SPNA248 March   2021 TM4C1292NCPDT , TM4C1292NCPDT , TM4C1292NCZAD , TM4C1292NCZAD , TM4C1294KCPDT , TM4C1294KCPDT , TM4C1294NCPDT , TM4C1294NCPDT , TM4C1294NCZAD , TM4C1294NCZAD , TM4C1299KCZAD , TM4C1299KCZAD , TM4C1299NCZAD , TM4C1299NCZAD , TM4C129DNCPDT , TM4C129DNCPDT , TM4C129DNCZAD , TM4C129DNCZAD , TM4C129EKCPDT , TM4C129EKCPDT , TM4C129ENCPDT , TM4C129ENCPDT , TM4C129ENCZAD , TM4C129ENCZAD , TM4C129LNCZAD , TM4C129LNCZAD , TM4C129XKCZAD , TM4C129XKCZAD , TM4C129XNCZAD , TM4C129XNCZAD

 

  1.   Trademarks
  2. Introduction
    1. 1.1 License
    2. 1.2 IwIP Version
    3. 1.3 lwIP Customization
    4. 1.4 IwIP API
      1. 1.4.1 TCP RAW APIs
      2. 1.4.2 UDP RAW APIs
    5. 1.5 lwIP Development Home Page and Support
  3. Application Examples
  4. Application Setup
    1. 3.1 Hardware Setup
    2. 3.2 Software Tools
  5. Download and Import the Ethernet examples
  6. Enet_tcpecho_server_lwip Example Overview
    1. 5.1 Build and Flash the Program
    2. 5.2 Check and Program the MAC Address
      1. 5.2.1 Using The LM Flash Programmer
      2. 5.2.2 Using the CCS
      3. 5.2.3 Using Uniflash
    3. 5.3 Configure the Terminal Window
    4. 5.4 Run the enet_tcpecho_server_lwip Example
  7. Enet_tcpecho_server_static_ip_lwip Example Overview
    1. 6.1 How to Configure lwIP for Static Address
    2. 6.2 Run the enet_tcpecho_server_static_ip_lwip Example
  8. Enet_udpecho_server_lwip Example Overview
    1. 7.1 Run the enet_udpecho_server_lwip Example
  9. Enet_dns_lwip Example Overview
    1. 8.1 How to Configure lwIP for DNS
    2. 8.2 How to View the DNS Traffic on Wireshark
    3. 8.3 Run the enet_dns_lwip Example
  10. Enet_sntp_lwip Example Overview
    1. 9.1 Run the enet_sntp_lwip Example
  11. 10Enet_tcpecho_client_lwip Example Overview
    1. 10.1 Configure the Server IP Address
    2. 10.2 Configure the SocketTest Server and Run the enet_tcpecho_client_lwip Example
    3. 10.3 Wireshark Capture for enet_tcpecho_client_lwip Example
  12. 11Enet_adcsensor_client_lwip Example Overview
    1. 11.1 Run the adcsensor_client_lwip Example
  13. 12Enet_udpecho_client_lwip Example Overview
    1. 12.1 Run the enet_udpecho_client_lwip Example
  14. 13References

Application Examples

The TivaWare library contains Ethernet examples that demonstrates creating HTTP web server applications based on lwIP stack. In this application report, the focus will be on demonstrating various echo-server and client applications. A collection of eight examples are presented here to show the TM4C129x MCU running with either the server applications or client applications.

Table 2-1 Application Examples
Example Type Description
enet_tcpecho_server_lwip Server An echo server application using TCP protocol. The server echoes back the packets received from the client. lwIP is configured to acquire the IP address from a DHCP server.
enet_tcpecho_server_static_ip_lwip Server An echo server application using TCP protocol but with lwIP configured for static IP address generation.
enet_updecho_server_lwip Server An echo server application using UDP protocol. The server echoes back the datagrams it receives from the client.
enet_dns_lwip Client A client application that requests the DNS (Domain Name Server) server to translate domains names into IP addresses, making it possible for the DNS clients to reach the origin server.
enet_sntp_lwip Client A client application that reports the current network time based on the SNTP (Simple Network Time Protocol).
enet_tcpecho_client_lwip Client An echo client application using TCP protocol. The client sends a greeting message to the server and echoes back the packets it receives from the server.
enet_adcsensor_client_lwip Client A client application that uses the on-chip ADC to periodically take the temperature reading of the device and send it to the server.
enet_udpecho_client_lwip Client An echo client application using UDP protocol. The client sends a greeting message to the server and echoes back the datagrams it receives from the server.