SPRUJ52C june 2022 – july 2023 AM69 , AM69A , TDA4AH-Q1 , TDA4AP-Q1 , TDA4VH-Q1 , TDA4VP-Q1
Descriptor starvation occurs when the Port attempts to fetch a free descriptor from an Rx Free Descriptor Queue or Rx Free Descriptor/Buffer Queue and none are available. When no descriptor is available, the Ring Accelerator will return a value of 0x0 for the descriptor pointer (Optionally, some ports may contain internal counters for the free queues which indicate how many elements are currently queued. In this case, no access to the RA is required and starvation is directly detected via a zero element count). When the port detects that descriptor starvation has occurred it will react based on the value of the RX_ERROR_HANDLING bit which was programmed into the Rx Flow N Configuration Register A.
The Port will assert a descriptor starvation indicator and will then return any descriptors that it has already used in the reception of the current packet back to the appropriate Free Descriptor or Free Descriptor/Buffer queue that they were fetched from. This is performed by writing the pointers for each descriptor to the Rx Free Descriptor Queue N Register in sequence using the queue indexes in the Rx DMA state. The port may choose to implement a counter that counts the number of packets that were dropped due to descriptor starvation and may also desire to distinguish between whether the starvation occurred on the packet descriptor (SOP) or on a buffer starvation.
The Port will assert a descriptor starvation indicator (which may cause an interrupt to the Host) and will then behave as if it had not performed the current data block transfer which caused the starvation. The Port is required to pause its current processing saving the state of the transfer. The next time that the channel comes into context it will again try to allocate a descriptor with the intention being that if buffers/descriptors have been added that the operation will complete successfully on a subsequent retry.