SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Send Call List

Note: This function is performed when a request is received to query the current calls list information from the the remote Hands-free device.

Description

The following function is responsible for sending the commands to send the Call Entry to a remote Hands-free Device. When received a request to query the remote current calls listfrom the remote Hands-free device. This function returns zero on successful execution and a negative value on all errors.

Parameters

The Send Call list command takes six parameters: Index, call direction, call status, call Mode, Multiparty, Phone Number (in the same order).

Command Call Examples

"SendCallList 0 1 1 0 0 5551212"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Send_Current_Calls_List(BluetoothStackID, CurrentClientPortID, &CurrentCallListEntry, Final)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Send_Current_Calls_List(unsigned int BluetoothStackID, unsigned int HFREPortID, HFRE_Current_Call_List_Entry_t*CurrentCallListEntry, Boolean_t FinalEntry)

Description of API

The following function is responsible for Sending Current Calls List Entries to the Remote Device. This function can only be performed by Audio Gateways that have received a requestto query the remote current calls list. This function accepts the Bluetooth Stack ID parameters for which the HFRE Port ID is valid as well as the HFRE Port ID. The thirdparameter to this function is the current call list entry to be sent. The final parameter to this function is a boolean indicating if this is the last call list entry to be sent therefore requiringthat an OK be sent as well. This function returns zero if successful or a negative return error code if there was an error.

Note: If the third parameter is specified as NULL, then the Final parameter *MUST* specify that this is the Final Entry. In this case, no call list entry can be sent, however, theterminating response can be sent.
Note: This function does not send the Phonebook Name as part of the Call List Entry. Use HFRE_Send_Current_Calls_List_With_Phonebook_Name if you wish to also send thePhonebook Name with the entry.