SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Set Microphone Gain

Description

The following function is responsible for setting the Microphone Gain on a Remote Device. This function returns zero on successful execution and a negative value on all errors. If theremote audio volume control feature is supported in the HF device than this can work.

Parameters

The command only requires an integer value for the MicroPhone Gain as the parameter.

Command Call Examples

  • "SetMicroPhoneGain 5"
  • "SetMicroPhoneGain 6"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Set_Remote_Microphone_Gain(BluetoothStackID, CurrentClientPortID, TempParam->Params->intParam)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Set_Remote_Microphone_Gain(unsigned int BluetoothStackID, unsigned int HFREPortID, unsigned int MicrophoneGain)

Description of API

This function is responsible for allowing synchronization and setting of the Remote Devices Microphone Gain. This function may only be performed if a valid Service Level Connectionexists. When called by a Hands-Free unit this function is provided as a means to inform the Remote Audio Gateway of the current Microphone Gain value. When called by an AudioGateway this function provides a means for the Audio Gateway to control the Microphone Gain of the Remote Hands-Free unit. This function accepts as its input parameters theBluetooth Stack ID for which the HFRE Port ID is valid as well as the HFRE Port ID. The final parameter is the Microphone Gain to be sent to the Remote Device. The Microphone GainParameter *MUST* be between the values of HFRE_MICROPHONE_GAIN_MINIMUM and HFRE_MICROPHONE_GAIN_MAXIMUM. This function returns zero if successful or anegative return error code if there was an error.