SWRA769 august   2023 CC2564C

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Demo Application
  5. 2Running the Bluetooth Code
  6. 3Server Set-Up Using HFP Demo Application
  7. 4Client Set-Up on the Demo Application
  8. 5Example: Audio Gateway with a Commercial Headset
  9. 6Application Commands
    1. 6.1  Generic Access Profile Commands
    2. 6.2  Help (DisplayHelp)
    3. 6.3  Inquiry
    4. 6.4  Pair
    5. 6.5  End Pairing
    6. 6.6  PIN Code Response
    7. 6.7  Pass Key Response
    8. 6.8  User Confirmation Response
    9. 6.9  Set Discoverability Mode
    10. 6.10 Set Connectability Mode
    11. 6.11 Set Pairability Mode
    12. 6.12 Change Simple Pairing Parameters
    13. 6.13 Get Local Address
    14. 6.14 Set Local Name
    15. 6.15 Get Local Name
    16. 6.16 Set Class of Device
    17. 6.17 Get Class of Device
    18. 6.18 Get Remote Name
  10. 7Hands-Free Profile Commands
    1. 7.1  Service Discovery
    2. 7.2  Open Audio Gateway Client
    3. 7.3  Manage Audio
    4. 7.4  Update Control Indicators
    5. 7.5  Call Waiting
    6. 7.6  Set Voice Recognition Activation
    7. 7.7  Set Speaker Gain
    8. 7.8  Set Microphone Gain
    9. 7.9  Disable Remote Sound Enhancement
    10. 7.10 Send Caller ID Notification
    11. 7.11 Set Ring Indication
    12. 7.12 Ring Indication
    13. 7.13 Send Incoming Call State
    14. 7.14 Close AG Client
    15. 7.15 Send Operator Info
    16. 7.16 Send Sub Number
    17. 7.17 Send Call List
  11. 8References
  12. 9Revision History

Call Waiting

Note: This function only works if the call waiting feature is supported in the remote HF device.

Description

The following function is responsible for sending a Call Waiting Notification to the Remote Hands-Free unit. This function returns zero on successful execution and a negative value on all errors. If the remote device call waiting feature is supported in the HF device than this works.

Parameters

The Call Waiting command takes only one parameter, which is the phone number to be sent as part of this response.

Command Call Examples

"CallWaiting +9198787899889"

Possible Return Values

  • (0) Command sent successfully
  • (-2) BTPS_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-4) FUNCTION_ERROR
  • (-8) INVALID_STACK_ID_ERROR
  • (-1000) BTHFRE_ERROR_INVALID_PARAMETER
  • (-1001) BTHFRE_ERROR_NOT_INITIALIZED
  • (-1002) BTHFRE_ERROR_INVALID_BLUETOOTH_STACK_ID
  • (-1003) BTHFRE_ERROR_LIBRARY_INITIALIZATION_ERROR
  • (-1004) BTHFRE_ERROR_INSUFFICIENT_RESOURCES
  • (-1005) BTHFRE_ERROR_INVALID_OPERATION
  • (-1006) BTHFRE_ERROR_INVALID_CODEC_ID

API Call

HFRE_Send_Call_Waiting_Notification(BluetoothStackID, CurrentClientPortID, TempParam->Params->strParam)

API Prototype

BTPSAPI_DECLARATION int BTPSAPI HFRE_Send_Call_Waiting_Notification(unsigned int BluetoothStackID, unsigned int HFREPortID, char *PhoneNumber)

Description of API

This function is responsible for Sending Call Waiting Notifications to the Remote Device. This function can only be performed by Audio Gateways which have Call Waiting Notification Enabled and have a valid Service Level Connection. This function accepts as its first input parameter the HFRE Port ID. The final parameter is the Phone Number required as one of the parameters within this response. This parameter is a pointer to a NULL terminated string (if specified) and must have a length less thanHFRE_PHONE_NUMBER_LENGTH_MAXIMUM. This function returns zero if successful or a negative return error code if there was an error.

Note: It is valid to either pass a NULL for the PhoneNumber parameter of a blank string to specify that there is no phone number present.