SWRU368C May 2018 – January 2021 CC3100 , CC3100MOD , CC3200 , CC3200MOD
If enabled, the SimpleLink performs an authentication check when the client first connects to the server. The authentication check can be enabled or disabled using the host API.
Authentication user name, password, and realm can also be configured by the host API.
By default, the authentication is disabled.
The default authentication values are:
A description of the host interface can be found in paragraph: Section 11.