SLUUCS1 October 2023 BQ25185
Connect the equipment as follows:
Power Supply PS #1: VIN of the BQ25185EVM at 5 V
Power Supply PS #2: VBAT of the BQ25185EVM at 3.7 V
Scope Channel SC#1: VIN at TP4
Scope Channel SC#2: VBAT at TP7
Scope Channel SC#3: VSYS at TP5
Procedure:
Connect 13 kOhm resistor using S1 switch box. Verify that the resistance from VSET/ILIM pin to GND is 13kOhm
This sets the battery regulation voltage to 4.2 V and the input current limit to 1100 mA
Measure the resistance from ISET to GND.
The resulting fast charge current will follow the equation:
Power on PS #1
Verify that the voltage at VSYS is about 4.5 V
Power on PS #2
Verify that current going into PS#2 is the configured charge current
Another method is to use the voltage at the ISET pin. The voltage at the ISET pin
To change the charge current:
Use the equation Ichg = 300/RIset (AΩ/Ω)
Measure the Resistance on the Iset pin
Adjust the R14 potentiometer to get the right RIset for your desired ICHG
Move the jumper on JP1 to the ADJ position
The ISET resistance should only be measured when the device is powered off but the ISET potentiometer can be adjusted during operation.
To adjust the charge voltage (VSET) and input current limit (ILim):
Refer to the VSET and IILIM table in the datasheet to see how the resistance on the IILIM pin affects the VBATREG and ILim
Adjust R15-R18 on S1 to set the correct resistance for your desired VSET and ILim
Turn off and on PS#1
The device will change the VSET/ILIM setting each time a new charge cycle is started (when VIN is plugged in and when /CE is pulled low).