SLUUCW9 December 2023 BQ76972
If measurement of an interconnect between cells is not practical or desired, the BQ76972 device also includes fixed settings for cell interconnect resistance in Settings:Interconnect Resistances:Cell 1 Interconnect – Cell 16 Interconnect in units of mΩ. The device subtracts the measured current times these interconnect resistance values from each differential cell voltage measurement before reporting the final cell voltage value.