SNAA393 January 2024 LMK6H
Always AC-couple the inputs of the PNA to prevent damaging the measurement equipment. If AC-coupling capacitors are not placed on the output of the clock source, a DC block can be used directly at the input of the PNA. Note that PNAs usually have an internal 50Ω termination to match the impedance of most coaxial cables. These are both important considerations when deciding how to terminate the clock source to maximize power and reduce signal reflections.
The following sections detail different measurement setups for TI's LMK6x family of oscillators.