Execute the ALP Setup Wizard program called “ALPF_setup_v_x_x_x.exe” that was extracted to a temporary location on the local drive of your PC.
There are 7 steps to the installation once the setup wizard is started:
- Select the "Next" button.
- Select “I accept the agreement” and then select the “Next” button.
- Select the location to install the ALP software and then select the “Next” button.
- Select the location for the start menu shortcut and then select the “Next” button.
- There will then be a screen that allows the creation of a desktop icon. After selecting the desired choices select the “Next” button.
- Select the “Install” button, and the software will then be installed to the selected location.
- Uncheck “Launch Analog LaunchPAD” and select the “Finish” button. The ALP software will start if “Launch Analog LaunchPAD” is checked, but it will not be useful until the USB driver is installed and board is attached.
Power the DS90UB960-Q1 EVM board with a 12 VDC power supply.