SPRABJ8B September   2022  – November 2023 AM2631 , AM2631-Q1 , AM2632 , AM2632-Q1 , AM2634 , AM2634-Q1 , AM263P4 , AM263P4-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. Introduction
    1. 1.1 Acronyms
  5. Power
    1. 2.1 Discrete DC-DC Power Solution
    2. 2.2 Integrated PMIC Power Solution
    3. 2.3 Power Decoupling and Filtering
    4. 2.4 Power Consumption
    5. 2.5 Power Distribution Network
      1. 2.5.1 Simulations
        1. 2.5.1.1 Core Digital Power 1.2 V
        2. 2.5.1.2 Digital/Analog I/O Power 3.3 V
    6. 2.6 e-Fuse Power
  6. Clocking
    1. 3.1 Crystal and Oscillator Input Options
    2. 3.2 Output Clock Generation
    3. 3.3 Crystal Selection and Shunt Capacitance
    4. 3.4 Crystal Placement and Routing
  7. Resets
  8. Bootstrapping
    1. 5.1 SOP Signal Implementation
    2. 5.2 OSPI/QSPI Memory Implementation
    3. 5.3 ROM OSPI/QSPI Boot Requirements
  9. JTAG Emulators and Trace
  10. Multiplexed Peripherals
  11. Digital Peripherals
    1. 8.1 General Digital Peripheral Routing Guidelines
  12. Analog Peripherals
    1. 9.1 General Analog Peripheral Routing Guidelines
      1. 9.1.1 Resolver ADC Routing Guidelines
  13. 10Layer Stackup
    1. 10.1 Key Stackup Features
  14. 11Vias
  15. 12BGA Power Fan-Out and Decoupling Placement
    1. 12.1 Ground Return
    2. 12.2 1.2 V Core Digital Power
      1. 12.2.1 Key Layout Considerations
    3. 12.3 3.3 V Digital and Analog Power
      1. 12.3.1 Key Layout Considerations
    4. 12.4 1.8 V Digital and Analog Power
      1. 12.4.1 Key Layout Considerations
  16. 13References
  17.   Revision History

Key Layout Considerations

  • Wide, minimum 15 mil traces, should be used for all power and ground return via fan-out.
  • 1.8 V digital and analog is generated from on-chip LDO and so is highly localized to the BGA pinout
  • A tightly coupled, adjacent ground return reference plane should be used for best transient performance and EMI coupling
  • Smaller power planes or wider traces should be used for minimal IR drop and best transient routing across the associated BGA pins
  • Smaller packaged, higher-frequency decoupling capacitance should be placed directly on BGA fan-out vias with as small of a dog-bone to power and ground return vias as possible
GUID-20220808-SS0I-1SHL-6DCR-K1JLRLLTHTW0-low.png Figure 12-12 AM263x controlCARD Excerpt – 1.8 V Digital Power Via Fan-Out and Plane Routing Layer 6
GUID-20220808-SS0I-GWGF-8FBB-CH1PSFTR7PSG-low.png Figure 12-13 AM263x controlCARD Excerpt – 1.8 V Digital Power Decoupling on Layer 10
GUID-20220808-SS0I-VCVN-CG9Q-5HDFJCP3MWXQ-low.png Figure 12-14 AM263x controlCARD Excerpt – 1.8 V Analog Power Via Fan-Out and Plane Routing Layer 6
Note: Figure 2-13 shows an example of a suboptimal routing between the FL12 filter output and the BGA pads. Ideally the output of the FL12 filter should be routed as a wide trace or small plane, and not smaller traces as was done on this initial revision of the controlCard EVM.
GUID-20220808-SS0I-Q22Z-LD1M-WKSVMTJXM0NC-low.png Figure 12-15 AM263x controlCARD Excerpt – 1.8 V Analog Power Decoupling on Layer 10