SPRACM9B June 2019 – November 2020 TMS320F28384D , TMS320F28384S , TMS320F28386D , TMS320F28386S , TMS320F28388D , TMS320F28388S , TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The setting up involves co-ordination between the debug environment and the SFRA GUI. Until getting familiar with connecting the SFRA GUIs to the target platform, it is a good idea to turn off the high voltage power input to the target platform.
The following initial steps can help with evaluating this build level:
These definitions inform the GUI about the starting value of noise frequency, number of different noise frequencies to sweep and the ratio between successive sweep frequencies, respectively. More information is available in the C2000™ Software Frequency Response Analyzer (SFRA) Library and Compensation Designer User's Guide associated with SFRA. In the context of this evaluation project, it is important to know and appreciate these parameters to tweak them for further repeat tests.
In this motor control project, SFRA can be performed on any of the three control loops such as the speed loop, D axis current loop and Q axis current loop. Technically, this could be performed on position loop as well, but is not included in this project scope and you can take it as an experiment, if desired.
The key steps can be explained as follows: