SPRU514Z July 2001 – October 2023 SM320F28335-EP
In order to track DP values across branches, the post-link optimizer requires that there are no indirect calls or branches, and all possible branch destinations have labels. If an indirect branch or call is encountered, the post-link optimizer will only track the DP value within a basic block. Branch destinations without labels may cause incorrect output from the post-link optimizer.
If the post-link optimizer encounters indirect calls or branches, it issues the following warning:
NO POST LINK OPTIMIZATION DONE ACROSS BRANCHES
Branch/Call must have labeled destinationThis warning is issued so that if the file is a hand written assembly file, you can try to change the indirect call/branch to a direct one to obtain the best optimization from the post linker.