SPRU514Z July 2001 – October 2023 SM320F28335-EP
If the compiler tools are to be installed in shared or read-only directory, mklib cannot build the standard libraries at link time; the libraries must be built before the library directory is made shared or read-only.
At installation time, the installing user must build all of the libraries which will be used by any user. To build all possible libraries, change the working directory to be the compiler RTS library directory 'lib' and invoke the mklib executable there:
mklib --allSome targets have many libraries, so this step can take a long time. To build a subset of the libraries, invoke mklib individually for each desired library.