TIDUDS9B December 2017 – November 2022
Set the current limit with the TPS27S00 device. As mentioned in Section 2.4.3, the current limit is set to 1 A. The current during the peak is limited to 1 A, as calculated in Equation 8.

Calculate the current in the switch during the ON state using Equation 9.

This calculated value for IOUT matches well with the value measured by the multimeter (see Figure 3-15 and Figure 3-16).
Figure 3-15 Inrush Current Measurement From
TPS27S100
Figure 3-16 Zoomed-In Shot of Inrush Current Measurement
From TPS27S100The two peaks that Figure 3-15 and Figure 3-16 show during the transition state corresponds to the current limit due to the input and output capacitance of the TIDA-00199 board. Path 1 and path 2 in Figure 3-17 show the two capacitances charging on the TIDA-00199 board.