SLVSA06K October 2009 – January 2022 DRV8824
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
Bulk capacitance sizing is an important factor in motor drive system design. It depends on a variety of factors including:
The inductance between the power supply and motor drive system limits the rate current can change from the power supply. If the local bulk capacitance is too small, the system responds to excessive current demands or dumps from the motor with a change in voltage. The designer must size the bulk capacitance to meet acceptable voltage ripple levels.
The data sheet generally provides a recommended value, but system-level testing is required to determine the appropriate-sized bulk capacitor.
Figure 9-1 Example Setup of Motor Drive System With External Power Supply