SLVSJP6 August 2025 ISOM8110-EP
ADVANCE INFORMATION
The ISOM8110-EP device can isolate both analog and digital signals due to the current-driven input stage. When supplied an input current (IF) of at least 0.7mA to the AN pin. This powers the internal modulator which includes the modulator and current sense blocks. The IF is sensed and converted into a high frequency carrier that is passed across the isolation barrier. Once demodulated on the secondary side of the device, this is used to bias the output transistor which tries to sink current from an external source into the COL pin (IC) proportional to the IF value. The ratio of IC to IF is the current transfer ratio (CTR).