SLVSJP6 August 2025 ISOM8110-EP
ADVANCE INFORMATION
The ISOM8110-EP opto-emulator is a single-channel, pin-to-pin upgrade for many traditional optocouplers. While standard optocouplers use an LED as the input stage, ISOM8110-EP uses an emulated LED as the input stage. The input and output stages are isolated by TI's proprietary silicon dioxide-based (SiO2) isolation barrier. This isolation technology makes ISOM8110-EP resistant to the wear-out effects found in optocouplers that degrade performance with increasing temperature, forward current, and device age. Ordering options include four different ranges of current transfer ratio (CTR).
The functional block diagram of ISOM8110-EP is shown in Section 7.2. The input signal is transmitted across the isolation barrier using an on-off keying (OOK) modulation scheme. The transmitter sends a high-frequency carrier across the barrier that contains information on how much current is flowing through the input pins. The receiver demodulates the signal after advanced signal conditioning and produces the signal through the output stage. This device also incorporates advanced circuit techniques to maximize bandwidth and minimize radiated emissions. Figure 7-2 shows conceptual details of how the OOK scheme works.