SNVSC55 September 2025 LM51770-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
For boost mode, the inductor selection is based on limiting the peak-to-peak current ripple, ΔIL, to approximately 20% of the maximum inductor current at the minimum input voltage. The target inductance for boost mode is:
For this application, an inductor with 1.8μH was selected.
Select the current sense resistor for the peak inductor current to not hit the over current limit at maximum output current. For that the peak inductor current needs to be calculated with the sum of the average and ripple current through the inductor.
The maximum peak to peak inductor current occurs at minimum input voltage and is given by:
The standard value of RCS = 1mΩ with 3 times 3mΩ is selected. With the 3 resistors in parallel it also reduces the parasitic inductance.
The maximum power dissipation in RCS happens at VIN(MAX):
Add a filter network to attenuate noise in the CSA and CSB sense lines. For most applications it is recommended to use a filter resistance RDIFF1 and RDIFF2 of 10Ω. Calculate the capacitance CDIFF for the filter with Equation 16. In this configuration 180pF is used.