SNVSC55 September 2025 LM51770-Q1
PRODUCTION DATA
Refer to the PDF data sheet for device specific package drawings
The LM51770-Q1 is designed to operate over a wide input voltage range. Enable compatibility of the characteristics of the input supply with the Absolute Maximum Ratings and Recommended Operating Conditions. In addition, enable the input supply to be capable of delivering the required input current to the fully loaded regulator. Use Equation 49 to estimate the average input current.
where
One way to get a value for the efficiency is the data from the efficiency graphs in Section 9.2.3 in the worst case operation mode. For most applications, the boost operation is the region of highest input current.
If the device is connected to an input supply through long wires or PCB traces with a large impedance, take special care to achieve stable performance. The parasitic inductance and resistance of the input cables have an adverse effect on converter operation. The parasitic inductance in combination with the low-ESR ceramic input capacitors form an under-damped resonant circuit. This circuit causes overvoltage transients at VIN each time the input supply is cycled ON and OFF. The parasitic resistance causes the input voltage to dip during a load transient. One way to solve such issues is to reduce the distance from the input supply to the regulator and use an aluminum or tantalum input capacitor in parallel with the ceramics. The moderate ESR of the electrolytic capacitors helps to damp the input resonant circuit and reduce any voltage overshoots. An EMI input filter is often used in front of the controller power stage. Unless carefully designed, this leads to instability as well as some of the previously mentioned effects.