SNVSC41 November 2023 LMR36500
PRODMIX
In some cases, an input UVLO level different than that provided internal to the device is needed. An input UVLO level different than that provided internal to the device is can be accomplished by using the circuit shown in Figure 8-3. The input voltage at which the device turns on is designated as VON while the turn-off voltage is VOFF. First, a value for RENB is chosen in the range of 10 kΩ to 100 kΩ, then Equation 13and Equation 14 are used to calculate RENT and VOFF, respectively.
where