SBOS701D December 2015 – August 2021 OPA191 , OPA2191 , OPA4191
PRODUCTION DATA
The OPAx191 family of operational amplifiers is manufactured using TI’s e-trim operation amplifier technology. This e-trim operational amplifier technology is a TI proprietary method of trimming internal device parameters during either wafer probing or final testing. Each amplifier input offset voltage and input offset voltage drift is trimmed in production, thereby minimizing errors associated with input offset voltage and input offset voltage drift. When trimming input offset voltage drift, the systematic or linear drift error on each device is trimmed to zero. Figure 7-1 illustrates this concept.
Figure 7-1 Input Offset Before and After Drift TrimA common method of specifying input offset voltage drift is the box method. The box method estimates a maximum input offset drift by bounding an offset voltage versus temperature curve with a box and using the corners of this bounding box to determine the drift. The slope of the line connecting the diagonal corners of the box corresponds to the input offset voltage drift. Figure 7-2 illustrates the box method concept. The box method works particularly well when the input offset drift is dominated by the linear component of drift, but because the OPA191 family uses TI’s e-trim operational amplifier technology to remove the linear component input offset voltage drift, the box method is not a particularly useful method of accurately performing an error analysis. Shown in Figure 7-2 are 30 typical units of OPAx191 with the box method superimposed for illustrative purposes. The boundaries of the box are determined by the specified temperature range along the x-axis and the maximum specified input offset voltage across that same temperature range along the y-axis. Using the box method predicts an input offset voltage drift of 0.9 µV/°C. As shown in Figure 7-2, the slopes of the actual input offset voltage versus temperature are much less than that predicted by the box method. The box method predicts a pessimistic value for the maximum input offset voltage drift and is not recommended when performing an error analysis.
Figure 7-2 The Box MethodInstead of the box method, a convenient way to illustrate input offset drift is to compute the slopes of the input offset voltage versus temperature curve. This is the same as computing the input offset drift at each point along the input offset voltage versus temperature curve. The results for the OPAx191 family are illustrated in Figure 7-3.
Figure 7-3 Input Offset Voltage Drift vs Temperature (SOIC Package)As illustrated in Figure 7-3, the input offset drift is typically less than ±0.3 µV/°C over the range from –40°C to +125°C. When performing an error analysis over the full specified temperature range, use the typical and maximum values for input offset voltage drift as described in the Electrical Characteristics tables. If a reduced temperature range is applicable, use the information illustrated in Figure 7-3 when performing an error analysis. To determine the change in input offset voltage, use Equation 1:
where
For example, determine the amount of OPA191ID input offset voltage change over the temperature range of 25°C to 75°C for 1 σ (68%) of the units. As shown in Figure 7-3, the input offset drift is typically 0.25 µV/°C. This input offset drift results in a typical input offset voltage change of (75°C – 25°C) × 0.25 µV/°C = 12.5 µV.
For 3 σ (99.7%) of the units, Figure 7-3 shows a typical input offset drift of approximately 0.75 µV/°C. This input offset drift results in a typical input offset voltage change of (75°C – 25°C) × 0.75 µV/°C = 37.5 µV.