SLVSJH6B July 2025 – December 2025 TLV3214-Q1
PRODMIX
The basic comparator configuration can produce a noisy "chatter" output if the applied differential input voltage is near the comparator offset voltage. This typically occurs when the input signal is moving very slowly across the switching threshold of the comparator. This problem can be prevented by adding external hysteresis to the comparator.
Since the TLV321x-Q1 devices only have 1.8mV of internal hysteresis, external hysteresis can be applied in the form of a positive feedback loop that adjusts the trip point of the comparator depending on the current output state. External hysteresis adds to the internal hysteresis.
The hysteresis transfer curve is shown in Figure 7-2. This curve is a function of three components: VTH, VOS, and VHYST:
Figure 7-2 Hysteresis Transfer CurveFor more information, please see the Comparator with and without hysteresis circuit aplication note.