SLVSH35A October 2023 – February 2024 TPS274C65CP
PRODUCTION DATA
If an application requires lower power dissipation than is possible with a 65-mΩ switch. Since the retry timer for each channel is not synchronized in TPS274C65CP, TI recommends to have the current limit for a single channel set higher than the total current for the paralleled channel. For example, if two of the channel are paralleled to drive 2A total current through the two channels, then the individual channel current limit needs to be set higher than 2A.
If the current limit cannot be set higher, a manual toggle of ENx (enable signals for the channels being paralleled) is needed after a thermal fault event happened.