JAJSJY1B September 2020 – March 2022 ADC3660
PRODUCTION DATA
The following FFT plots show the performance of THS4541 driving the ADC3660 operated at 65 MSPS with a full-scale input at -1 dBFS. The first FFT spectrum below shows the performance with a single tone input at FIN = 1 MHz and decimation by 16 (real).
The second FFT spectrum shows the a single tone input at FIN = 5 MHz and complex decimation by 16 where the NCO is programmed to 4.5 MHz.
Decimation by 16, real |
Decimation by 16, complex, NCO = 4.5 MHz |