JAJSOS2B February 2021 – September 2022 CC2652PSIP
PRODUCTION DATA
In order to meet the module power-on-reset requirements, an external 0.1 µF capacitor is required on the nRESET pin during power ON. In addition, VDDS (Pin 46) and VDDS_PU (Pin 47) should be connected together. If the reset signal is not based upon a power-on-reset and is derived from an external MCU, then the external capacitor will not be needed and VDDS_PU (Pin 47) should be No Connect (NC). Please refer to Figure 10-1 for the recommended circuit implementation and Table 10-1 for the recommended 0.1 µF capacitor.