JAJSNS3A October 2015 – February 2023 DLPA3005
PRODUCTION DATA
The switching of the three LED NMOS switches (P, Q, R) is controlled such that a switch is returned to the OPEN position first before the subsequent switch is set to the CLOSED position (BBM), Figure 7-7. The dead time between opening and closing switches is controlled through the BBM register. Switches that already are in the CLOSED position and are to remain in the CLOSED state, are not opened during the BBM delay time.