JAJSE49B August 2017 – February 2018 DRV10987
PRODUCTION DATA.
If the motor is spinning in the reverse direction, the DRV10987 device provides several methods to convert it back to the forward direction.
One method, reverse drive, allows the motor to be driven so that it accelerates through zero velocity. The motor achieves the shortest possible spin-up time in systems where the motor is spinning in the reverse direction.
If this feature is not selected, then the DRV10987 device may be configured either to wait for the motor to stop spinning or to brake the motor. After the motor has stopped spinning, the motor start-up sequence proceeds as it would for a motor which is stationary.
Take care when using the reverse-drive or brake feature to ensure that the current is limited to an acceptable level and that the supply voltage does not surge as a result of energy being returned to the power supply.
Figure 16. Start the Motor Under Different Initial Conditions