JAJSRS8I February 2007 – November 2023 LM5116
PRODUCTION DATA
The bootstrap capacitor (CHB) between the HB and SW pins supplies the gate current to charge the high-side MOSFET gate at each cycle turn-on as well as supplying the recovery charge for the bootstrap diode (D1). These current peaks can be several amperes. The recommended value of the bootstrap capacitor is at least 0.1 µF, and must be a good quality, low ESR, ceramic capacitor located at the pins of the IC to minimize potentially damaging voltage transients caused by trace inductance. The absolute minimum value for the bootstrap capacitor is calculated as:
where
CHB is typically less than 5% of VCC. A value of 1 µF was selected for this design.