JAJSEA6B December 2017 – February 2019 LMH5401-SP
PRODUCTION DATA.
The LMH5401-SP is a decompensated, fully-differential amplifier (FDA) configurable with external resistors for noise gain greater than 4 V/V or 12 dB (GBP = 6.5 GHz). For most of this document, data are collected for Gv = 17 dB for both single-ended-to-differential (SE-DE) and differential-to-differential (DE-DE) conversions in the diagrams illustrated in the Test Schematics section. When matching the output to a 100-Ω load, the evaluation module (EVM) uses external 40-Ω resistors to complete the output matching, as the device has an internal series 10 Ω on each output. Having on-chip output resistors creates two potential reference points for measuring the output voltage. The amplifier output pins create one output reference point (OUT_AMP). The other output reference point is OUT_LOAD at the 100-Ω load impedance, RL. These points are illustrated in Figure 53; see also the Test Schematics section.
Most measurements in the Electrical Characteristics tables and in the Typical Characteristics sections are measured with reference to the OUT_AMP reference point. Equation 1 shows that the conversion between reference points is a straightforward reduction of 3 dB for power and 6 dB for voltage in a matched condition when Ro is set such that 20 Ω + 2 × Ro = RL. With Ro set to 40 Ω and RL set to 100 Ω-differential, the total load impedance seen by the amplifier, RLtotal, is 200 Ω. This is considered a matched load condition as 100-Ω is driving RL of 100 Ω. The device is also capable of driving lower impedances. By setting Ro to 0 Ω, RLtotal becomes 120 Ω. This is considered an unmatched condition since 20 Ω is driving RL of 100 Ω. As explained in the Application Curves section, efficiency is improved (losses reduced) in a mismatched condition which is acceptable if transmission line reflections are avoided and proper termination practices are employed. As stated previously, most measurements in this document are referenced to OUT_AMP node. However, there are some typical characteristic plots that are measured with a fixed signal swing with respect to the OUT_LOAD reference point; specifically, IMD3 Figure 25 and Figure 27 are referenced to the voltage swing at node OUT_LOAD.
This document makes references to both voltage gain, Gv, and power gain, Gp. Voltage gain is defined as the ratio of the differential output voltage at node OUT_AMP to the differential, or single-ended, input voltage at the node before Rg. Power gain, for the purposes of this document, is defined as the ratio of the power dissipated on RL (100 Ω-differential) to the power transferred from a source to the input impedance of the amplifier. Whereas voltage gain contains no input and load impedances in its calculation, power gain does depend on termination impedances.