JAJSNB3 September 2023 LP5813
PRODUCTION DATA
The LP5813 integrates 4 high-side PMOS scan switches and 4 constant current sinks. Each OUTx (x = 0, 1, 2, 3) has 1 PMOS scan switch and 1 constant current sink. The source of PMOS switches are connected to the boost output VOUT. During normal operation at default setting, the switches turn on sequentially from OUT0 to OUT3. At the same time, only one OUT is selected working as switch, the other 3 OUTs act as constant current sink. Thus a 4×3 matrix is formed with ¼ multiplexing ratio. The scanning order of OUTs can be configured in 'Dev_config_2' register
Figure 9-3 shows the simplified TCM scheme timing diagram of the four outputs. A complete display frame includes 4 sub-periods. Each sub-period contains dimming period and blank time period. In switching period, 1 output is selected as switch and the other 3 OUTs are selected as current sinks. Blank time is applied between two adjacent switching periods for ghosting elimination.
One sub-period cycle time Tsub is calculated as Equation 4:
One complete frame time Tframe is calculated as Equation 5:
The LP5813 can be configured to direct-drive mode, TCM-drive mode and mix-drive mode by the 'led_mode' bits in 'Dev_Config_1' register. The mix-drive mode contains both direct drive mode and TCM-drive mode for different outputs. With this method, the LP5813 can provide the maximum flexibility for LED configurations of LED average current, LED count, and PCB layouts.