JAJSMU9B August 2021 – February 2022 MCT8316A
PRODUCTION DATA
To prevent sudden changes in the torque applied to the motor which could result in acoustic noise, the MCT8316A device provides the option of limiting the maximum rate at which the speed command can change. The closed loop acceleration rate parameter sets the maximum rate at which the speed command changes (shown in Figure 8-31). In the MCT8316A, closed loop acceleration rate is configured through CL_ACC.