JAJSGD8B October 2018 – Sept 2019 TMUX1574
PRODUCTION DATA.
The tON (VDD) time is defined as the time taken by the output of the device to rise to 90% after the supply has risen past the supply threshold. The 90% measurement is used to provide the timing of the device turning on in the system. Figure 33 shows the setup used to measure turn on time, denoted by the symbol tON (VDD).
the tOFF (VDD) time is defined as the time taken by the output of the device to fall to 90% after the supply has fallen past the supply threshold. The 90% measurement is used to provide the timing of the device turning off in the system. Figure 33 shows the setup used to measure turn off time, denoted by the symbol tOFF (VDD).
Figure 33. tON (VDD) and tOFF (VDD)Time Measurement Setup