JAJSGD8B October 2018 – Sept 2019 TMUX1574
PRODUCTION DATA.
Propagation delay is defined as the time taken by the output of the device to rise or fall 50% after the input signal has risen or fallen past the 50% threshold. Figure 35 shows the setup used to measure propagation delay, denoted by the symbol tPD.
Figure 35. Propagation Delay Measurement Setup